Keysight 89600 VSA .NET API
MarkersLimitTestResult Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : MarkersLimitTestResult Enumeration


Glossary Item Box

The result of a limit test

Syntax

Visual Basic (Declaration) 
Public Enum MarkersLimitTestResult 
   Inherits System.Enum
C# 
public enum MarkersLimitTestResult : System.Enum 
C++/CLI 
public enum class MarkersLimitTestResult : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FailLimit test failed.—
NoneNo test result available (test was not run).—
PassLimit test passed.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also