Keysight 89600 VSA .NET API
MarkersPeakOrder Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : MarkersPeakOrder Enumeration


Glossary Item Box

Specifies the order of the peak markers.

Syntax

Visual Basic (Declaration) 
Public Enum MarkersPeakOrder 
   Inherits System.Enum
C# 
public enum MarkersPeakOrder : System.Enum 
C++/CLI 
public enum class MarkersPeakOrder : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
XThe peak order is by the X-axis.—
YThe peak order is by the Y-axis.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also