Keysight 89600 VSA .NET API
MathFunctionSyntaxResult Class Members
See Also  Properties  Methods 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : MathFunctionSyntaxResult Class

Glossary Item Box

The following tables list the members exposed by MathFunctionSyntaxResult.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorMathFunctionSyntaxResult ConstructorInitializes a new instance of the MathFunctionSyntaxResult class with the specified error message and error position.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyErrorMessageGets the error message.  —
Public PropertyErrorPositionGets the position of the error.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodSerialize  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also