| Visual Basic (Declaration) | |
|---|---|
Public Function New( _ ByVal obj As IRemoteNotifyCollectionChanged _ ) | |
| C# | |
|---|---|
public NotifyCollectionChangedWrapper( IRemoteNotifyCollectionChanged obj ) | |
| C++/CLI | |
|---|---|
public: NotifyCollectionChangedWrapper( IRemoteNotifyCollectionChanged^ obj ) | |
Parameters
- obj
- The remote object to monitor for CollectionChanged events.
When using this constructor, monitoring of the remote object will not start until a handler is connected to the CollectionChanged event exposed by this wrapper.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)