Keysight 89600 VSA .NET API
NotifyPropertyChangedWrapper Constructor(IRemoteNotifyPropertyChanged)
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > NotifyPropertyChangedWrapper Class > NotifyPropertyChangedWrapper Constructor : NotifyPropertyChangedWrapper Constructor(IRemoteNotifyPropertyChanged)


obj
The remote object to monitor for PropertyChanged events.

Glossary Item Box

Initializes a new instance of the NotifyPropertyChangedWrapper class that will monitor the supplied remote object for PropertyChanged events.

Syntax

Visual Basic (Declaration) 
Public Function New( _
   ByVal obj As IRemoteNotifyPropertyChanged _
)
C# 
public NotifyPropertyChangedWrapper( 
   IRemoteNotifyPropertyChanged obj
)
C++/CLI 
public:
NotifyPropertyChangedWrapper( 
   IRemoteNotifyPropertyChanged^ obj
)

Parameters

obj
The remote object to monitor for PropertyChanged events.

Remarks

When using this constructor, monitoring of the remote object will not start until a handler is connected to the PropertyChanged event exposed by this wrapper.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also