Keysight 89600 VSA .NET API
PageOrientationType Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : PageOrientationType Enumeration


Glossary Item Box

Define the orientation of the printed content on the media.

Syntax

Visual Basic (Declaration) 
Public Enum PageOrientationType 
   Inherits System.Enum
C# 
public enum PageOrientationType : System.Enum 
C++/CLI 
public enum class PageOrientationType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
LandscapeLandscape orientation—
PortraitPortrait orientation—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also