Keysight 89600 VSA .NET API
PlaybackPeriodicSyncStyle Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : PlaybackPeriodicSyncStyle Enumeration


Glossary Item Box

Represents the style (source) of the periodic sync trigger.

Syntax

Visual Basic (Declaration) 
Public Enum PlaybackPeriodicSyncStyle 
   Inherits System.Enum
C# 
public enum PlaybackPeriodicSyncStyle : System.Enum 
C++/CLI 
public enum class PlaybackPeriodicSyncStyle : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AutoFree run trigger.—
RecordingTriggerRecording trigger.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also