Keysight 89600 VSA .NET API
PowerReferencePlane Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : PowerReferencePlane Enumeration


Glossary Item Box

Specifies what reference plane to use for level and power calculations when using the baseband IQ inputs.

Syntax

Visual Basic (Declaration) 
Public Enum PowerReferencePlane 
   Inherits System.Enum
C# 
public enum PowerReferencePlane : System.Enum 
C++/CLI 
public enum class PowerReferencePlane : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BasebandAssumes that the reference plane desired is the direct baseband inputs to the ADCs and does not filter away the negative frequency components or scale the data like what is normally done for RF zoom measurements.—
RFAssumes the signal had been frequency converted and low pass filtered in such a way that the negative frequency components of the signal have been removed and then the I and Q parts have had a gain of 2 applied so that the voltage levels reflect the original signal magnitude. The data will be processed so that the power is reflective of what the original RF signal power was before the frequency conversion (assuming no conversion loss). (i.e. that the reference plane is at the RF side of the frequency conversion).—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.40

See Also