Keysight 89600 VSA .NET API
PxiTrigger Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : PxiTrigger Enumeration


Glossary Item Box

Specifies which PXI backplane trigger to use.

Syntax

Visual Basic (Declaration) 
Public Enum PxiTrigger 
   Inherits System.Enum
C# 
public enum PxiTrigger : System.Enum 
C++/CLI 
public enum class PxiTrigger : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Pxi0PXI Trigger #0—
Pxi1PXI Trigger #1—
Pxi2PXI Trigger #2—
Pxi3PXI Trigger #3—
Pxi4PXI Trigger #4—
Pxi5PXI Trigger #5—
Pxi6PXI Trigger #6—
Pxi7PXI Trigger #7—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also