Keysight 89600 VSA .NET API
ResolutionBandwidthMetric Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : ResolutionBandwidthMetric Enumeration


Glossary Item Box

Specifies the metric to use when specifying the resolution bandwidth

Syntax

Visual Basic (Declaration) 
Public Enum ResolutionBandwidthMetric 
   Inherits System.Enum
C# 
public enum ResolutionBandwidthMetric : System.Enum 
C++/CLI 
public enum class ResolutionBandwidthMetric : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
EquivalentNoiseEquivalent noise bandwidth—
Minus3DB-3 dB Bandwidth—
Minus6DB-6 dB Bandwidth—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also