Keysight 89600 VSA .NET API
Create Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > ResultCollection Class : Create Method


Glossary Item Box

Create a new instance of the Result class and add it to the collection.

Overload List

OverloadDescription
Create()Create a new instance of the Result class and add it to the collection.  
Create(String)Create a new instance of the Result class and add it to the collection.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also