Keysight 89600 VSA .NET API
SequencedPlaybackMode Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : SequencedPlaybackMode Enumeration


Glossary Item Box

Specifies the mode used for sequencing measurements using recording playback.

Syntax

Visual Basic (Declaration) 
Public Enum SequencedPlaybackMode 
   Inherits System.Enum
C# 
public enum SequencedPlaybackMode : System.Enum 
C++/CLI 
public enum class SequencedPlaybackMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
IndependentSpecifies independent recording playback for sequenced measurements.—
TimeTrackingSpecifies the measurement with the earliest current position (relative to start position) has priority in sequencing, to support time tracking between playback measurements.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.40

See Also