Keysight 89600 VSA .NET API
SequentialTrackingMode Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : SequentialTrackingMode Enumeration


Glossary Item Box

Specifies what kind of sequential input tracking mode to use for the input channels.

Syntax

Visual Basic (Declaration) 
Public Enum SequentialTrackingMode 
   Inherits System.Enum
C# 
public enum SequentialTrackingMode : System.Enum 
C++/CLI 
public enum class SequentialTrackingMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
NoneSequential tracking is disabled—
TimePhaseUse a tracking channel to adjust the time and phase relative to a reference channel—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.20

See Also