| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property AmplitudeInVolts As Double | |
| C# | |
|---|---|
public virtual double AmplitudeInVolts {get; set;} | |
Source output amplitude is set as volts peak. This property is an alternative to Amplitude which sets the output level in dBm as the power of the voltage across a 50 ohm load.
For an arbitrary waveform generator (AWG), this property gets or sets the maximum instantaneous output voltage of the downloaded waveform.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.40