| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property Delay As Double | |
| C# | |
|---|---|
public virtual double Delay {get; set;} | |
This property is used to deskew source channels. The start of waveform playback on the source channel is delayed by the time specified.
The IsSupported("Delay") method can be used to determine whether this property is supported or not with the current Source.SelectedHardware.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.40