Keysight 89600 VSA .NET API
AmplitudeInVolts Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Source Class : AmplitudeInVolts Property


Glossary Item Box

Gets or sets the source output amplitude in volts for all channels.

Syntax

Visual Basic (Declaration) 
Public Overridable Property AmplitudeInVolts As Double
C# 
public virtual double AmplitudeInVolts {get; set;}
C++/CLI 
public:
virtual property double AmplitudeInVolts {
   double get();
   void set (    double value);
}

Remarks

Source amplitude may be controlled individually per channel. When queried, this property always returns the value for the first channel.

Source output amplitude is set as volts peak. This property is an alternative to Amplitude which sets the output level in dBm as the power of the voltage across a 50 ohm load.

For an arbitrary waveform generator (AWG), this property gets or sets the maximum instantaneous output voltage of the downloaded waveform.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.40

See Also