| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub Connect() | |
| C# | |
|---|---|
public virtual void Connect() | |
| C++/CLI | |
|---|---|
public: virtual void Connect(); | |
When Connect is called, the source hardware is reset and then set up according to the other Source object properties. Some of the property values may be clipped to valid values depending on the source hardware capabilities.
Connected state has no effect on the value of the Enabled property of SourceChannel.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.60