| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub Disconnect() | |
| C# | |
|---|---|
public virtual void Disconnect() | |
| C++/CLI | |
|---|---|
public: virtual void Disconnect(); | |
When Disconnect is called, the state of the source hardware may be changed by using its front panel, or by another program using the API, so the Source properties do not necessarily reflect the state of the source hardware.
Connected state has no effect on the value of the Enabled property of SourceChannel.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.60