| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property GlobalTriggerType As SourceGlobalTriggerType | |
| C# | |
|---|---|
public virtual SourceGlobalTriggerType GlobalTriggerType {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property SourceGlobalTriggerType GlobalTriggerType { SourceGlobalTriggerType get(); void set ( SourceGlobalTriggerType value); } | |
GlobalTrigger trigger type is a mode of trigger operation supported by some multiple channel sources that starts phase coherent waveform play. This property sets the type of trigger that is used to initiate the global trigger.
The IsSupported("GlobalTriggerType") method can be used to determine whether this property is supported or not with the current Source.SelectedHardware.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.60