Keysight 89600 VSA .NET API
SelectedHardware Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Source Class : SelectedHardware Property


Glossary Item Box

Gets or sets the source hardware to use.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SelectedHardware As HardwareConfiguration
C# 
public abstract HardwareConfiguration SelectedHardware {get; set;}
C++/CLI 
public:
abstract property HardwareConfiguration^ SelectedHardware {
   HardwareConfiguration^ get();
   void set (    HardwareConfiguration^ value);
}

Remarks

The hardware configuration set must have a type of Source or Awg when this property's value is not null.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also