Keysight 89600 VSA .NET API
TriggerAction Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Source Class : TriggerAction Property


Glossary Item Box

Gets or sets the action that is initiated by the trigger

Syntax

Visual Basic (Declaration) 
Public Overridable Property TriggerAction As SourceTriggerAction
C# 
public virtual SourceTriggerAction TriggerAction {get; set;}
C++/CLI 
public:
virtual property SourceTriggerAction TriggerAction {
   SourceTriggerAction get();
   void set (    SourceTriggerAction value);
}

Remarks

The IsSupported("TriggerAction") method can be used to determine whether this property is supported or not with the current Source.SelectedHardware.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.60

See Also