Keysight 89600 VSA .NET API
TriggerType Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Source Class : TriggerType Property


Glossary Item Box

Gets or sets the type of trigger that starts the waveform playing on all source channels

Syntax

Visual Basic (Declaration) 
Public Overridable Property TriggerType As SourceTriggerType
C# 
public virtual SourceTriggerType TriggerType {get; set;}
C++/CLI 
public:
virtual property SourceTriggerType TriggerType {
   SourceTriggerType get();
   void set (    SourceTriggerType value);
}

Remarks

Changing trigger type from Immediate to another type pauses waveform playback until a trigger of the newly selected type occurs.

The IsSupported("TriggerType") method can be used to determine whether this property is supported or not with the current Source.SelectedHardware.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.60

See Also