Keysight 89600 VSA .NET API
WaveformAdjustmentMode Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Source Class : WaveformAdjustmentMode Property


Glossary Item Box

Gets or sets the desired behavior when the ARB waveform does not meet the MinWaveformPoints and WaveformLengthQuantum requirements.

Syntax

Visual Basic (Declaration) 
Public Overridable Property WaveformAdjustmentMode As WaveformAdjustmentMode
C# 
public virtual WaveformAdjustmentMode WaveformAdjustmentMode {get; set;}
C++/CLI 
public:
virtual property WaveformAdjustmentMode WaveformAdjustmentMode {
   WaveformAdjustmentMode get();
   void set (    WaveformAdjustmentMode value);
}

Remarks

Returns WaveformAdjustmentMode.ExtendWithZeros if no source is connected or value cannot be determined. Use IPropertyInfo.ValidValues<T> to check which values are supported (can check once Connected = true).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.60

See Also