Keysight 89600 VSA .NET API
ColorCount Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Spectrogram Class : ColorCount Property


Glossary Item Box

Gets or sets the number of color levels for the spectrogram / 3D map.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property ColorCount As Integer
C# 
public abstract int ColorCount {get; set;}
C++/CLI 
public:
abstract property int ColorCount {
   int get();
   void set (    int value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also