Keysight 89600 VSA .NET API
IsFirstAuto Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Spectrogram Class : IsFirstAuto Property


Glossary Item Box

Gets or sets a value indicating whether the first (top) scan is automatically determined (not from the First property).

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsFirstAuto As Boolean
C# 
public abstract bool IsFirstAuto {get; set;}
C++/CLI 
public:
abstract property bool IsFirstAuto {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also