| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property MaxCount As Integer | |
| C# | |
|---|---|
public abstract int MaxCount {get; set;} | |
The maximum value is limited by the amount of memory in your computer. The spectrogram memory is used to:
- Refresh the spectrogram when you change trace properties.
- Save the spectrogram when you save the data to a file.
- Read the data when you access data on a specified scan.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)