| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property TraceSelect As Integer | |
| C# | |
|---|---|
public abstract int TraceSelect {get; set;} | |
If IsTraceSelectVisible is True, then this property selects the current scan on a spectrogram trace. All normal or delta markers are shown on the current scan. Also, if another trace is showing the same result as this trace, then that trace shows the current scan.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)