Keysight 89600 VSA .NET API
ActualEquivalentSweepTime Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SpectrumFrequencyChannel Class : ActualEquivalentSweepTime Property


Glossary Item Box

Gets the actual equivalent sweep time of the measurement.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property ActualEquivalentSweepTime As Double
C# 
public abstract double ActualEquivalentSweepTime {get;}
C++/CLI 
public:
abstract property double ActualEquivalentSweepTime {
   double get();
}

Remarks

When IsEquivalentSweepTimeAuto is set to true then this will reflect the current equivalent sweep time that the measurement has chosen to use.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also