Keysight 89600 VSA .NET API
ActualVideoBandwidth Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SpectrumFrequencyChannel Class : ActualVideoBandwidth Property


Glossary Item Box

Gets the actual video bandwidth for cases when it may differ from the desired video bandwidth. This normally occurs when using gating with a manually entered gate length where the gate length is longer than what is needed for the current VBW/RBW ratio. This property is only supported when the ActiveInputDomains has a value of InputDomains.Time. This property will return a value of double.NaN when not supported.

Syntax

Visual Basic (Declaration) 
Public Overridable ReadOnly Property ActualVideoBandwidth As Double
C# 
public virtual double ActualVideoBandwidth {get;}
C++/CLI 
public:
virtual property double ActualVideoBandwidth {
   double get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.60

See Also