Keysight 89600 VSA .NET API
DefaultSpan Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SpectrumFrequencyChannel Class : DefaultSpan Method


Glossary Item Box

Sets the Span to its default value, which is the largest span supported by the current hardware.

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub DefaultSpan() 
C# 
public abstract void DefaultSpan()
C++/CLI 
public:
abstract void DefaultSpan(); 

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also