Keysight 89600 VSA .NET API
IsVideoBandwidthToResolutionBandwidthRatioAuto Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SpectrumFrequencyChannel Class : IsVideoBandwidthToResolutionBandwidthRatioAuto Property


Glossary Item Box

Gets or sets a value indicating whether the VideoBandwidthToResolutionBandwidthRatio property is automatically set.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsVideoBandwidthToResolutionBandwidthRatioAuto As Boolean
C# 
public abstract bool IsVideoBandwidthToResolutionBandwidthRatioAuto {get; set;}
C++/CLI 
public:
abstract property bool IsVideoBandwidthToResolutionBandwidthRatioAuto {
   bool get();
   void set (    bool value);
}

Remarks

When true, the VideoBandwidthToResolutionBandwidthRatio property is set to 1.0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also