Keysight 89600 VSA .NET API
Points Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SpectrumFrequencyChannel Class : Points Property


Glossary Item Box

Gets or sets the number of points produced by each detector.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Points As Integer
C# 
public abstract int Points {get; set;}
C++/CLI 
public:
abstract property int Points {
   int get();
   void set (    int value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also