Keysight 89600 VSA .NET API
SetCenterSpan Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SpectrumFrequencyChannel Class : SetCenterSpan Method


center
Specifies the center frequency value, in Hertz.
span
Specifies the frequency span value, in Hertz.

Glossary Item Box

Set the measurement center frequency and span.

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub SetCenterSpan( _
   ByVal center As Double, _
   ByVal span As Double _
) 
C# 
public abstract void SetCenterSpan( 
   double center,
   double span
)
C++/CLI 
public:
abstract void SetCenterSpan( 
   double center,
   double span
) 

Parameters

center
Specifies the center frequency value, in Hertz.
span
Specifies the frequency span value, in Hertz.

Remarks

This method sets the measurement's center frequency and span all at one time with only a single measurement restart. That is faster than setting each property individually which would cause multiple measurement restarts.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also