Keysight 89600 VSA .NET API
SetStartStopFrequency Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SpectrumFrequencyChannel Class : SetStartStopFrequency Method


startFrequency
Measurement start frequency in Hz.
stopFrequency
Measurement stop frequency in Hz.

Glossary Item Box

Set the measurement Start and Stop frequency properties all at one time.

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub SetStartStopFrequency( _
   ByVal startFrequency As Double, _
   ByVal stopFrequency As Double _
) 
C# 
public abstract void SetStartStopFrequency( 
   double startFrequency,
   double stopFrequency
)
C++/CLI 
public:
abstract void SetStartStopFrequency( 
   double startFrequency,
   double stopFrequency
) 

Parameters

startFrequency
Measurement start frequency in Hz.
stopFrequency
Measurement stop frequency in Hz.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also