Keysight 89600 VSA .NET API
SpectrumGateSetupApi Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : SpectrumGateSetupApi Enumeration


Glossary Item Box

Specifies what part of the API is currently being used for the spectrum gate trigger setup.

Syntax

Visual Basic (Declaration) 
Public Enum SpectrumGateSetupApi 
   Inherits System.Enum
C# 
public enum SpectrumGateSetupApi : System.Enum 
C++/CLI 
public enum class SpectrumGateSetupApi : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
InputTriggerSetup is done via the Measurement.Input.Trigger API.—
SpectrumGateSetup is done via the Measurement.Spectrum.Gate API.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.60

See Also