| Visual Basic (Declaration) | |
|---|---|
Public Overloads MustOverride Function Value( _ ByVal key As String, _ ByVal defaultValue As Single _ ) As Single | |
| C# | |
|---|---|
public abstract float Value( string key, float defaultValue ) | |
| C++/CLI | |
|---|---|
public: abstract float Value( String^ key, float defaultValue ) | |
Parameters
- key
- The key.
- defaultValue
- The returned value if the key is not found or the value cannot be converted to a float.
Return Value
The float value.See Item for more information about keys.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)