Keysight 89600 VSA .NET API
Value(String,String) Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > StateDictionary Class > Value Method : Value(String,String) Method


key
The key.
defaultValue
The returned value if the key is not found or the value cannot be converted to a string.

Glossary Item Box

Returns the string value associated with the specified key.

Syntax

Visual Basic (Declaration) 
Public Overloads MustOverride Function Value( _
   ByVal key As String, _
   ByVal defaultValue As String _
) As String
C# 
public abstract string Value( 
   string key,
   string defaultValue
)
C++/CLI 
public:
abstract String^ Value( 
   String^ key,
   String^ defaultValue
) 

Parameters

key
The key.
defaultValue
The returned value if the key is not found or the value cannot be converted to a string.

Return Value

The string value.

Remarks

See Item for more information about keys.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also