Keysight 89600 VSA .NET API
StatusBits Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : StatusBits Enumeration


Glossary Item Box

The measurement status bits.

Syntax

Visual Basic (Declaration) 
Public Enum StatusBits 
   Inherits System.Enum
C# 
public enum StatusBits : System.Enum 
C++/CLI 
public enum class StatusBits : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AcquiringThe measurement is acquiring data—
AdcOverloadThe measurement hardware input channel has over-ranged.—
AverageCompleteThe measurement average is complete.—
CalibratingCalibration is in progress.—
CalibrationNeededCalibration is needed.—
CalibrationWarmUpInstrument is warming up; frequent calibration may be needed.—
EndDataRecording playback reached the end of the recording data. This only happens when playback looping is disabled.—
ExternalReferenceLockThe hardware is locked to the external reference.—
GapDataThere is a gap between the last scan and the current scan of data.—
InternalReferenceLockThe hardware is locked to the internal reference.—
MeasurementDoneMeasurement is done.—
MeasuringThe measurement is not paused (i.e. it is running).—
NoneNo status bits are set.—
PulseNotFoundNo pulse is found by the (demodulation) measurement.—
RangingA measurement auto range is in progress.—
ReadingDataThe measurement is reading the acquisition data from the hardware.—
RecordingThe measurement is recording data.—
SettlingThe measurement is acquiring the settle data (before the measurement data).—
StaleDataRestarting measurement acquisition because the data is stale (too old).—
SyncNotFoundNo sync is found by the (demodulation) measurement.—
TestFailA test (e.g. LimitTest) has failed.—
VisibleThe application window is visible—
WaitPreTriggerThe measurement is acquiring pre-trigger data.—
WaitReferenceLockThe measurement is waiting for a frequency reference lock.—
WaitTriggerThe measurement is waiting for the trigger event.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

You can query the state of each of these status bits from the Measurement.Status property.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also