Keysight 89600 VSA .NET API
PathsPerAcquisition Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Switch Class : PathsPerAcquisition Property


Glossary Item Box

Gets the number of Switch paths to use (connect up) per acquisition. Set the value using ChangePathConfiguration

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property PathsPerAcquisition As Integer
C# 
public abstract int PathsPerAcquisition {get;}
C++/CLI 
public:
abstract property int PathsPerAcquisition {
   int get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also