Keysight 89600 VSA .NET API
InputChannelIndex Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SystemCalibrationResult Class : InputChannelIndex Property


Glossary Item Box

Gets the index of the physical channel that was calibrated

Syntax

Visual Basic (Declaration) 
Public ReadOnly Property InputChannelIndex As Integer
C# 
public int InputChannelIndex {get;}
C++/CLI 
public:
property int InputChannelIndex {
   int get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also