Keysight 89600 VSA .NET API
TraceDataSelect Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : TraceDataSelect Enumeration


Glossary Item Box

Specifies which data is selected.

Syntax

Visual Basic (Declaration) 
Public Enum TraceDataSelect 
   Inherits System.Enum
C# 
public enum TraceDataSelect : System.Enum 
C++/CLI 
public enum class TraceDataSelect : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
XThe X-axis data is selected.—
XYBoth the X-axis and Y-axis data are selected.—
YThe Y-axis data is selected.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also