Keysight 89600 VSA .NET API
TraceTableFormat Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : TraceTableFormat Enumeration


Glossary Item Box

Specifies the format used to display the symbol binary bit data in the Symbol Table.

Syntax

Visual Basic (Declaration) 
Public Enum TraceTableFormat 
   Inherits System.Enum
C# 
public enum TraceTableFormat : System.Enum 
C++/CLI 
public enum class TraceTableFormat : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BinaryBinary format.—
HexadecimalHexadecimal format (if there are enough bits/symbol).—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also