Keysight 89600 VSA .NET API
TriggerOut Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : TriggerOut Enumeration


Glossary Item Box

Specifies the trigger out choice.

Syntax

Visual Basic (Declaration) 
Public Enum TriggerOut 
   Inherits System.Enum
C# 
public enum TriggerOut : System.Enum 
C++/CLI 
public enum class TriggerOut : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
OffNo trigger out will be generated.—
Out1Enable trigger out on the connector designated to be the first trigger out connected.—
Out2Enable trigger out on the connector designated to be the second trigger out connected.—
Out3Enable trigger out on the connector designated to be the third trigger out connector.31.00
Out4Enable trigger out on the connector designated to be the fourth trigger out connector.31.00
Pxi0Enable trigger out on the PXI trigger 0 back plane line—
Pxi1Enable trigger out on the PXI trigger 1 back plane line—
Pxi2Enable trigger out on the PXI trigger 2 back plane line—
Pxi3Enable trigger out on the PXI trigger 3 back plane line—
Pxi4Enable trigger out on the PXI trigger 4 back plane line—
Pxi5Enable trigger out on the PXI trigger 5 back plane line—
Pxi6Enable trigger out on the PXI trigger 6 back plane line—
Pxi7Enable trigger out on the PXI trigger 7 back plane line—
UnknownThe hardware connected has not specified to the application whether it generates a trigger out or not.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also