Keysight 89600 VSA .NET API
TriggerPeriodicSyncSource Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : TriggerPeriodicSyncSource Enumeration


Glossary Item Box

Specifies the periodic trigger sync source (how first measurement is triggered).

Syntax

Visual Basic (Declaration) 
Public Enum TriggerPeriodicSyncSource 
   Inherits System.Enum
C# 
public enum TriggerPeriodicSyncSource : System.Enum 
C++/CLI 
public enum class TriggerPeriodicSyncSource : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
ExternalSpecifies that periodic trigger synchronizes with the external trigger.—
FreeRunSpecifies that periodic trigger does not synchronize with another trigger.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also