Keysight 89600 VSA .NET API
CommandLineArgsSupportedKey Field
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > VersionInfo Class : CommandLineArgsSupportedKey Field


Glossary Item Box

The key for the capability that indicates what VSA application command line arguments are supported. The value returned is a single string that contains a list of the command line arguments separated by a space in between each and where each is the uppercase name of the command line argument supported.

Syntax

Visual Basic (Declaration) 
Public Const CommandLineArgsSupportedKey As String
C# 
public const string CommandLineArgsSupportedKey
C++/CLI 
public:
const String^ CommandLineArgsSupportedKey

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also