Keysight 89600 VSA .NET API
GrpcPhysicsHardwareSupportedKey Field
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > VersionInfo Class : GrpcPhysicsHardwareSupportedKey Field


Glossary Item Box

The key for the capability that indicates whether the VSA application supports connecting to "physics" API based hardware using the gRPC physics API. The string value associated with this key can be parsed into a boolean.

Syntax

Visual Basic (Declaration) 
Public Const GrpcPhysicsHardwareSupportedKey As String
C# 
public const string GrpcPhysicsHardwareSupportedKey
C++/CLI 
public:
const String^ GrpcPhysicsHardwareSupportedKey

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also