Keysight 89600 VSA .NET API
VirtualSignalCollection Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : VirtualSignalCollection Class


Glossary Item Box

This collection contains the set of VirtualSignal objects representing the settings for each virtual signal in a source channel.

Object Model

VirtualSignalCollection ClassVirtualSignal Class

Syntax

Remarks

The collection will be empty for source channels that do not support virtual signals.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also