Keysight 89600 VSA .NET API
WindowType Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : WindowType Enumeration


Glossary Item Box

Specifies the type of windowing.

Syntax

Visual Basic (Declaration) 
Public Enum WindowType 
   Inherits System.Enum
C# 
public enum WindowType : System.Enum 
C++/CLI 
public enum class WindowType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BlackmanHarrisSpecifies Blackman Harris window.17.00
FlatTopSpecifies Flat Top window.—
GaussianSpecifies Gaussian window.17.00
GaussianTopSpecifies Gaussian Top window.—
HanningSpecifies Hanning window.—
KaiserBesselSpecifies Kaiser-Bessel window.17.00
UniformSpecifies Uniform window. This has the same effect as no window.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also