Keysight 89600 VSA .NET API
SetExtension Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.VsaInternal Namespace > IExtensible Interface : SetExtension Method


extensionType
allowed type of extension to set

Glossary Item Box

Sets the extension to the desired extensionType.

Syntax

Visual Basic (Declaration) 
Function SetExtension( _
   ByVal extensionType As Type _
) As Object
C# 
object SetExtension( 
   Type extensionType
)
C++/CLI 
Object^ SetExtension( 
   Type^ extensionType
) 

Parameters

extensionType
allowed type of extension to set

Return Value

the instance of the extension that was created

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also