| Class | Description | |
|---|---|---|
![]() | CalculationControl | The CalculationControl represents the measurement control for the DirectCalculation. |
![]() | CalculationResult | The CalculationResult contains all the possible results provided by the DirectCalculation. |
![]() | ConfigurationResult | The ConfigurationResult represents the results of the configure operation of the DirectCalculation. |
![]() | LteDirectCalculation | This class provides the members required to configure and control a DirectCalculation. |
![]() | RequirementsForOfdmDomainInputData | The RequirementsForOfdmDomainInputData represents the requirements for the ofdm domain input data. |
![]() | RequirementsForTimeDomainInputData | The RequirementsForTimeDomainInputData represents the requirements for the time domain input data. |
| Enumeration | Description | |
|---|---|---|
![]() | CyclicPrefixLength | Enum values indicating the cyclic prefix length for DirectCalculation. |
![]() | InputDataDomain | Enum values indicating the input data domain for DirectCalculation. |